Southco - Connect. Create. Innovate.
Home About Us Contact Us
  My Account: Login
  Search:   
  
 
Language
Glossary
Click on the letters below to find alphabetical listings of definitions for standard Southco terms and phrases.
A | B | C | D | E | F | G | H | I | J | K | L | M | N | O | P | Q | R | S | T | U | V | W | X | Y | Z

1/4 Turn Fasteners

A fastener with a formed head stud and lobes at the end of the stud, that fastens to (or unfastens from) a receptacle when the stud is rotated in a 1/4 turn (90 degrees) position.
A
Actuation
The movement of the pawl of a latch into the latched/unlatched position.

Actuator
Generally the handle or the part of a latch that rotates or slides the pawl (retainer) into its locked/unlocked position.

Actuator - Hex Socket
One of a type of actuator that requires a hex shaped tool to rotate the latch pawl into locked/unlocked position.

Adjustable
For latches or door handles: having the ability to adapt to varying panel thicknesses. For Hinges: having multi-positional capability, having the ability to regulate/dampen the opening/closing speed, and/or having the ability to regulate the amount of gasket compression around the door or frame.

Adjustable Compression Hinge
A hinge that has the ability to regulate amount of gasket compression around a door frame.

Adjustable Draw Latch
A latch and/or door handle having: a) the ability to adapt to varying panel thicknesses
(usually by changing the latch pawl position), or b) the ability to regulate the amount of gasket compression around a door frame.

Adjustable Grip Latches
A latch having: a) the ability to adapt to varying panel thicknesses, b) ability to regulate amount of gasket compression around a door frame.

Adjustable Hinges
A hinge that has ability to regulate (dampen) opening/closing speed and/or has multi-positional capability.

Average Ultimate Load
The load that causes failure or excessive deformation which renders the product inoperable.

back to top ^
B
Bail Head (Stud)
Type of stud (1/4 turn) in which the head has a supplemental ring (bail) attached. The bail ring is used for ease of manipulating the stud. The bail can pivot into a flat, out-of-way position.

Base Plate
Generally referred to as the latch mounting plate. It can be riveted or screw mounted to the panel.
May also refer to the portion of a latch assembly that houses or holds the latch body.

Blade
A reciprocating plate on rotary type, tension, or over-center draw latches that, when combined with a stationary catch plate (keeper), provides tensional clamping forces to draw and hold panels or objects securely, while offering vibration resistance.

Blind
Typically refers to a type of installation in which the fastener is not viewable from the far side of the mounting panel after it has been installed. May also apply in situations where a fastener is installed without access to the back side of panel. This is considered a "blind hole" installation.

Blind Hole
A type of panel preparation in which the mounting hole does not extend through the mounting panel. Used for "blind" fastener application.

Break-away Load
The minimum load required to break the latching force between door and its door frame.

Built-in Drag Feature
An integral mechanism that creates frictional retention without having to apply supplementary external forces. It prevents "backlashing" "sudden unexpected release" or "flopping" of latch and/or door.

Bushing
Used in "Swell Latches". The rubber gasket that expands radially to close off the inner panel hole, while drawing inner and outer panels together.



back to top ^
C
Captive
Being retained in the panel after installation, and during and after use.

Captive Screw Fastener
A type of fastener whose components are retained in the outer panel when the threaded portion is
unfastened from mating component.

Catch
A component of the latch arrangement that provides for latch pawl retention.

Magnetic Catch
A type of flat latch plate that provides a means of magnetic attraction, allowing a magnetic-type latch
to retain a door or panel in the closed position.

Centerline
The center of a fastener, the center of a rotating locking mechanism, or center location of mounting
hole(s) in installation panel.

Clamping Force
The force exerted by a latch to draw two panels together. Also called PULL-UP FORCE.

Click-Stop
Pre-set positioning feature that allows a fastener or hinge to rotate into fractional positions and is able to hold a panel or door in the full/partial opened position. Also called DETENT.

Clinching
A term used to describe a rivet's ability to grasp joined mating panels as it is installed,
providing a solid joint.

Compression Latch
A latch that performs two sequential functions: a) the pawl first swings into the latching position behind the door frame by turning the latch handle, knob or head, and b) then draws the pawl towards the frame, compressing the door frame gasket and/or door panel against door frame with additional turn(s) of the latch head. The amount of compression applied an be fixed or adjustable.

Cup/Cup Latch
An adjustable or compression latch with a cupped face plate that allows the actuation handle to lie in the recessed area. It provides a flush appearance without any protruding parts.

back to top ^

D
Dampened Door Swing
The closing rate of a door/panel is controlled, such that door will close gradually versus slamming shut. An adjustable hinge with frictional or BUILT-IN DRAG feature can provide this.

Detent
A pre-set internal positioning feature that allows a fastener or hinge to rotate into fractional positions and/or to hold panel(s) or door(s) in full/partial opened position. Also used to indicate full open/closed position of some latching mechanisms. In hinges, also called HOLD OPEN FEATURE.

Door-retaining Spring
A Southco latch that consists of a rotating, heavy gauged, helical spring that forms a mechanical means of retaining and/or locking a panel or door in the opened or closed position.

Door Thickness Range
The minimum/maximum door thickness required between the latching mechanism and retaining pawl that will allow for effective latching and retention.

Drive Recess
A recessed configuration (Hex, Slotted, Phillips, Lobed, TORX®, Toolhead® etc.) in the head of a latch and/or fastener that requires a specially designed tool to install, remove or operate the product.

Dust and Moisture Seal
A cap or gasket that is used to prevent dust and moisture from entering into latch components.


back to top ^
E
Effective Rod Length
For 2- and 3-point latching: the predetermined length of actuation rod(s) that will provide for equally applied latching forces at all points of a 2 point, 3 point, rod and roller, or remote compression latching system.

Ejector Spring
Spring used in Retractable or SPRING EJECTED type fasteners. It enables the screw thread to fully retract
from the mating panel.

EMI/RFI Shielding
The capability to reduce the transmission of electromagnetic or radio energy into or out of an enclosure.

Enclosure
The portion of a cabinet that provides storage area. Also refers to the portion of a cabinet surrounding the door frame.

Engaged
The state where the pawl or retaining mechanism of a latch is rotated into position such that full retention of
door or panel is achieved.

Escutcheon
Generally a protective plate (metal or plastic) that surrounds the key-lock portion of a latch. Sometimes used for decorative purposes to cover mounting screws on the face of a door/panel. Also called Escutcheon Plate.

Environmental Gasketing
Gasketing designed to prevent leakage of environmental elements (i.e. dust, moisture, etc).

back to top ^

F
Ferrule
On Captive or retractable screws, the part that houses the screw body, and is captivated to the panel during installation. Also called "Stand off".

Flange
The raised edge surrounding the latch cup (that houses the latch body) that forms a collar for retaining the latch against the door/panel when latch is installed in its mounting hole.

Float
The term used to define the ability to move freely within a constrained area or feature (i.e. hole) and is used to allow for panel misalignment.

Flush
Not extending beyond the surface of panel or door enclosure.

Fractional Turn Fasteners
A fastener similar to 1/4 turn fasteners, except that it uses a two-part cam (stationary and moving) and a
rubber sleeve (bushing). When the moving cam is rotated along the stationary cam by turning
the stud, it compresses and radially expands the rubber sleeve thereby closing off the inner panel
hole and drawing the inner and outer panels together. The rate of "fractional turn" is determined by panel thicknesses, in a through-hole application, and, by the diameter of the hole in the inner panel
of a blind hole application.

Frame
Enclosure surrounding an access panel or door.

Fully-retracting Stud Assembly
Having the capability to retract the threaded portion of a fastener (stud) away from the mating panel by means of an internal spring, while retaining the fastener to the mounted panel. Generally relates to captive type screw or nut. Also called SPRING EJECTED stud.

back to top ^

G
Gap
Spatial distance between two mating components.

Gasket
A ring, strip, or sheet of rubber, metal, or other material, that when used under applied pressure, will seal off gas,
fluid, dust, etc. Also called O-RING.

Grip
The nominal total panel thickness for which a fastener is to be used. (This is usually customer defined).

Grip Length
The effective length in terms of screw thread engagement, screw length, stud length, rivet shank length, etc., that will accommodate a defined panel thickness range and provide for effective latching or panel retention.

Grip Range
The minimum/maximum distance between the latching mechanism and retaining panel as defined by amount of pawl travel that will allow for proper latching and retention. May also be called PANEL THICKNESS RANGE.

Guide/Guide Brakcet
A component part of a 2-point, 3-point, remote, or rod and roller compression system that guides the actuation rods through a linear motion to provide equal compression at all latching points. Also referred to as Rod Guide.

back to top ^

H
Hidden Panel-latch System
A slam-action panel latch system. The entire latching mechanism and system components are installed on the inside of a door panel, leaving a clean, unblemished outer surface panel.

Hinge

Door-positioning Hinge
A Hinge that has special DETENT feature which allows it to hold a door open in a variety of preset positions.

Free-swinging Hinge
A hinge that allows door to swing freely with no hindrance.

Lift-off Hinge
Any of a variety of hinges that allows for easy removal of a door from a cabinet, without having to remove the mounted hinge(s). The same hinge components can also be installed in the inverted position so as not to permit "lift-off" feature.

Hole Plug
A device generally made of plastic or other synthetic material, used for closing or sealing off recessed or through-holes in a panel. (Used extensively in appliance applications)

Housing
Generally referring to the "body" portion of a latch assembly that holds the internal actuating components.

back to top ^

I
Insertion Force
Also referred to as INSTALLATION FORCE, it is the initial force required to properly install a fastener.

Installation
The means by which a fastener, hinge, captive screw, etc. is affixed to the door, frame, or panel.

Press-in Installation (Generally for Captive Screw Fasteners):
The procedure for installing a fastener into a slightly undersized hole in the panel by means of mechanical press.

Flare-in Installation (Generally for Captive Screw Fasteners):
The procedure for installing fastener into a hole having a radially flared (countersink) edge.
A special back-up tool must be used to secure the fastener in the hole by flaring the ferrule (stand-off) behind the panel.

Floating Installation (Generally for Captive Screw Fasteners):
The procedure for installing fastener into a hole with a special back-up tool. Fastener ferrule (stand-off) is secured in the panel while the threaded stud is able to float radially. This allows for misalignment of inner and outer panel holes.

Snap-in Installation (Generally for Captive Screw Fasteners):
The procedure for installing a fastener into a through-hole in the panel. The fastener is secured in panel by a lip feature on the ferrule that snaps in place when fully installed in panel.

Thread-in Installation (Generally for Captive Screw Fasteners):
The procedure for installing a threaded fastener into a hole with mating thread.

P.C. Board Installation (Generally for Captive Screw Fasteners):
Applies to installing a fastener into p.c. boards. Generally uses PRESS-IN installation.

back to top ^

J
Jam Nut
For latch applications, it is generally a hex nut threaded onto the actuation shaft and positioned on
one or both sides of pawl. It restrains the pawl from linear or axial movement along the shaft, and secures panel retention.

back to top ^
K
Keeper/Keeper Plate
The mating component in a draw latch arrangement that creates tension against the latching rod,
plate, or spring to provide retaining function.

Concealed Keeper
A type of keeper, offered on a variety of draw-latches that remains concealed behind latch handle
when latch is fully engaged.

Fixed Keeper
Available with the Hidden Panel Latching System. The keeper has a fixed keeper stud mounted on it.
It allows for only minimal panel/door misalignment. This style of keeper is intended for lift-off panel application.

Floating Keeper
Available with the Hidden Panel Latching System. This keeper has an oversized keeper stud mounting hole and special "u-bent" washer designed to assist panel/door misalignment. This style of keeper is intended for hinge-type panel application.

Reversed Keeper
One of several keeper plate options available on Over-Center draw latches, where the mounting hole position is reversed from traditional keeper styles, so that the mounting hardware is concealed by the latch blade

Right-Angled Keeper
A keeper bracket having an "L" shaped configuration such that the retaining mechanism is positioned 90 degrees to the door panel and frame.

Key-actuated Operated
Any latching arrangement requiring a key (or special tool) to perform latching/unlatching operations and/or retain latch in locked position.

Keylock
Built-in latch feature that provides for security. A key is required to unlock and rotate latch mechanism.

Knuckle
Each of two mating halves of a "Lift-off" or "Compression" type hinge. Generally referred to as either
the "upper" or "lower" knuckle.

Fixed Knuckle
The knuckle that is mounted in the stationary position (on the door frame) is referred to as the "fixed knuckle" and is generally the half having the pin on which the mating knuckle pivots. The location where the "fixed knuckle" is mounted is referred to as the "fixed position".

In-line Style Hinge Knuckle Mounting
Type of hinge mounting where the door is flush against or in-line with the door frame.

Offset Knuckle Style Hinge Mounting
Type of hinge mounting used to accommodate most instances where the door is not positioned flush against
or in-line with the door frame.

Knurl
An external surface feature consisting of a series of small projections or ridges applied to a screw head or knob to provide a means for gripping or holding the part.

back to top ^

L
Latches-
Draw Latch
Any of a variety of latches that is designed to draw and hold two panels together.

Flush Latch
A latch designed to have minimal or no protrusion from the face of the mounting panel.

Flexible Latch
Refers to a draw-type latch in which the main component is manufactured from rubber or elastomer material. Generally designed for use in applications where vibration isolation or panel misalignment is of concern.

Paddle Latch
A latch having a flat, flip-out handle feature for actuating the latch.

Remote Latch
A latching system where the latching forces are exerted at some arbitrary distance from the actuator.
This applies to single and multi-point latching systems.

Slam Action Latch
A type of latch that requires handle actuation to open and pushing or slamming of the door to close.

Latching Rod
The adjustable part of an adjustable draw latch that provides the reach in the unlatched position and
draw-up tension in latched position.

Leaf
A major component that makes up one half of a fixed-hinge arrangement. One hinge generally has two of them.

L-Handle
A single-piece latch handle having an "L" shaped configuration.

Lift-off Panel
Refers to a panel/door set up in a removable configuration.

back to top ^

M
Material and Finish
The base (primary) material used in the product and any supplementary coating (i.e. zinc chromate,
chrome, black oxide, etc.) applied to provide protection from moisture, rust, etc. and to enhance product appearance.

Mating Thread
The internally or externally threaded hole designed to mate with a threaded stud having the same thread
diameter and thread pitch.

Maximum Work Load
The maximum recommended load at which the product continues to function properly.

Misalignment
Having incorrect alignment between mating features.

Mounting Options-
Concealed Mounting

Type of mounting where the latching mechanism and mounting hardware are concealed behind the panel.
(Example: Hidden-Panel Latch)

Edge Mounting
Type of mounting associated with installing the latching mechanism on the edge of the mating panels.
(Example: Butt-Joint Panel Fastener)

Face Mounting
Type of mounting associated with mounting latching mechanism on the front or face of the panel.
Typical for most latching applications.

Flush Mounting
Situation in which mounting hardware is affixed where panels are flush or in-line.

Side Mounting
Type of mounting where the latching mechanism and keeper are mounted on the backside of connecting
panels and not are viewable from front of cabinet. (Example: Butt-Joint Panel Fastener)

Single-Hole Mounting
Type of mount where complete mounting of the latching mechanism or access hardware is performed in a s
single hole in panel face.

back to top ^

O
Offset Door
Condition where the door is not positioned flush against, or in-line with, the mating door frame.
A hinge arrangement using an "offset style mounting" would be used for this type of application.

Operation/Actuation Force
The ergonomically designed force required to effectively operate or actuate a latch or fastener from the
"open-to-closed" or "unfastened-to-fastened" position.

O-ring
A circular gasket generally made of natural or synthetic rubber compound, that is used for sealing
applications to prevent entry and/or leaking of fluids, air, moisture, dust, etc.

back to top ^

P
Panel Preparation
Suggested layout of mounting holes for proper latch installation into panel, door, enclosure, etc.

Panel Thickness Range
The minimum/maximum distance between the latching mechanism and retaining panel as defined by
amount of pawl travel that will allow for proper latching and retention. May also be called GRIP RANGE.

Pawl
The rotary feature that provides door/panel retention when actuated into position. In some cases, this feature also provides gasket compression. Generally has either straight or offset configuration and has linear adjustability along rotating shaft to accommodate a variety of panel thicknesses.

Curved Pawl
The pawl has a concave/convex curvature on the working end.

Flat Pawl
The pawl has a flat (no curvature) on the working end.

Pawl Indicator
A marking or other indicator on a latch knob that indicates the position and/or the opened or closed status
of the latching mechanism and/or pawl.

Press-in
Relating to a type of fastener capable of being installed in a slightly undersized hole using minimal force.

Product Class
Southco's identification of the family of latch, fastener, or other access hardware. The first two characters of the part number define the "product class".

Pull
A kind of access hardware with features such as a handle or finger pull used in opening cabinet doors, drawers, etc. Varieties include one-piece units and latch/pull combinations.

Pull Tab
A supplemental component that integrates the latch mechanism and a pull handle in a latch arrangement.

Pull-up Action
The mechanical advantage provided by a latch in drawing two panels together. The action can be in a linear, co-planer, perpendicular, or axial form.

Pull-up Force
The force exerted by a latch to draw two panels together. Also referred to as CLAMPING FORCE.

back to top ^

Q
Quick-opening Captive Screw
A screw type fastener with a square profile thread that allows the fastener to engage and disengage a
panel or receptacle with only a few turns.

back to top ^
R
Receptacle
The mating part that accepts a 1/4-Turn stud and provides for positive fastening.
Note: This is a critical feature when designing in a 1/4-Turn fastener.

Recommended Mounting Direction
The suggested spacing or location of hole(s) to install a latch assembly or latch and keeper arrangement,
in order to ensure proper latch operation and performance.
(Note: This is suggested information only. Actual mounting hole location may vary depending on customer's specific application, but may affect actual latch performance.)

Rivet-
Drive Rivet
A type of fastener, generally installed with a hammer or pneumatic tool to drive the pin into the shank
of the rivet. Generally used for retaining thin or thick walled panels together.

Blind Riveting
An application in which a DRIVE RIVET is used to retain a thin panel to a thick panel by means of installing
into a BLIND HOLE in the thick panel.

back to top ^

S
Secondary Catch

A device on draw-type latches that provides supplementary locking for added security.

Self Adjusting
Able to adjust the latching mechanism and maintain retention capability without mechanical means of adjustment (i.e. wrenching, screwing, etc.). This is usually accomplished by natural decompression of internally compressed spring.

Separation Line
A line of reference for the designer, where mating surfaces (i.e. base/lid, case/lid, cover/base, door/frame) exist. This line correlates the panel separation to the recommended latch mounting location.

Shaft
The rod-shaped component found in most compression-type and draw-type latches that provides latch actuation. The shaft also provides for linear and axial positioning of the latch pawl.

Spring Ejected
Having the capability to retract the threaded portion of a (usually captive screw) fastener away from the mating panel by means of an internal spring.

Spring Loaded
Having a spring installed into the assembled unit where latching force is provided by natural decompression of the compressed spring. Used in spring-loaded plunger, slam latches.

Steady State Clamp Force
A known constant force (tensile or compression) applied to the product over a specified length of time.

Stud Ejector
A spring-action mechanism designed to separate a stud from its receptacle, ferrule, or panel.

Swell Latch
A compression-type latch with a rubber bushing that, when the handle is actuated, expands radially to close
off the inner panel hole while drawing the inner and outer panels together. Features include: a) thin, thick and blind wall applications, b) accommodates misalignment between door and frame, and c) has excellent vibration resistance characteristics.

back to top ^

T
Tab, finger grip
A protruding feature that provides a pull and a gripping surface to ease opening and closing of door/panel.

Tamper Resistant Access
An application in which a specific tool or key is required to actuate a latch. In tamper-resistant rivet applications, it can indicate evidence of tampering.

T-bar
A type of handle having a "T"-shape configuration that provides a more positive grip for rotary actuation.

T-handle
A single-piece handle having a "T"-shaped configuration

Tightening Torque
The maximum recommended torque to be applied to the mounting hardware (i.e. nuts, jamnuts, mounting screws, etc.). Tightening torque should not exceed recommended values, or latch damage/failure may occur.

Toggle Action
Feature on Over-center and Under-center draw latches that mechanically identifies full positive
latching condition.

Tool-operated
Refers to a fastener/latch that requires a specific tool (or key) to mates with the drive recess in the fastener head or latch handle in order to perform latching and unlatching operations.

Tool Secured
An application where the latch retains the door/panel in a locked state. A specific tool (or key) is required to unlock the latch.

Total Material thickness
Combined or total thickness of mating panel(s); panel, frame, gasket, and gap.

Two / three point latching system
A latching arrangement having latching and/or compression capabilities in two or three areas of a door and frame. Assembly generally includes actuator rods and an operating latch.

Type A/Type B
Generally describes right- or left-handed operation and/or installation of latches or hinges.

back to top ^
U
Ultimate Shear Strength
Forces exerted in opposite directions as in a cutting action, which renders the product inoperable.

back to top ^